Vybrid GPIO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid GPIO

跳至解决方案
1,223 次查看
ogj
Contributor IV

I'm using a Vybrid MVF61NN151CMK50 processor (Emcraft SOM) and having some weird issues with the GPIO pins. I'm trying to drive some LEDs. The cathode of the LED goes to the 3.3V supply. The anode goes to a resistor (270 ohm) and from there to an IO pin. All of the GPIO clocks are on, the IOMUX registers for these pins are set to 0x00002502 (OBE enabled, open drain enabled, 37 ohm drive, med speed, alt func = 0. The problem is that the LEDs are always on. It doesn't matter whether the PDOR shows the pin high or low. It's like the pulldown transistor won't turn off.

I have a similar situation just trying to drive a GPIO pin high. In this case the IOMUX register is set to 0x00000102 (OBE enabled, 37 ohm drive). The pin is always low, regardless of the value in the PDOR register. What am I missing? 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,054 次查看
ogj
Contributor IV

I found the problem. I didn't realize that there is not a 1:1 correspondence between GPIOA and GPIO Port 0. For instance GPIOB0 is controlled by Port0 Pin 22. I thought that GPIOA was GPIO0.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,055 次查看
ogj
Contributor IV

I found the problem. I didn't realize that there is not a 1:1 correspondence between GPIOA and GPIO Port 0. For instance GPIOB0 is controlled by Port0 Pin 22. I thought that GPIOA was GPIO0.

0 项奖励
回复