Vybrid GPIO on /sys/class/gpio does not switch properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid GPIO on /sys/class/gpio does not switch properly

6,911 Views
johannestraxler
Contributor III

I have a GPIO (PTE8 - Pin Nr. 113) exported via the /sys/class/gpio device tree and configured as OUTPUT direction.

From my C-Code I do the following

int fd = open ("/sys/class/gpio/gpio113/value", O_WRONLY);

...

while (1)

{

     ...

     write (fd, "1", 1);

     ...

     ...

     write (fd, "0", 1);

     ...

}

The problem is, that write() does not work every time. It seems as if the value is not written into the Port-Register of the processor. I did measurements with a scope directly on the processor pin and the value showed 1 after the second write statement in line 11, but it should be 0. In the same step I checked in shell with "cat /sys/class/gpio/gpio113/value" and here the value is also shown as 0. When I then typed "echo 0 > /sys/class/gpio/gpio113/value" in the shell the pin went to 0. I also tried to modify the driver strength in IOMUX to 25Ohm, 50Ohm and 150Ohm and explicitely set OBE to high, but the behaviour is the same - sometimes it work - sometimes not!

Do you have an advice for me?

Thanks in advance,

Johannes

Labels (2)
12 Replies

6,018 Views
falstaff
Senior Contributor I

Hi Johannes,

What Kernel version do you exactly use? The Mainline GPIO/Pinctrl driver behaves slightly different then the 3.0/3.13 Timesys one. Also, how do you debug exactly? At least on current kernels, it looks like the value write could sleep. Do you break the code execution after the write?

Linux/drivers/gpio/gpiolib-sysfs.c - Linux Cross Reference - Free Electrons

What polarity do you use? (see active_low file). However, I don't think this is the issue since you do not change it and hence it should be the same issue when using sysfs from the shell.

--

Stefan

0 Kudos
Reply

6,018 Views
johannestraxler
Contributor III

Hi Stefan,

I'm using

Linux version 3.0.15-ts-armv7l

gcc version 4.8.3 (Timesys 20140811) )

PREEMPT

In this case I didn't have to debug, it was enough to write a shell script, which toggles the pin and verified it with an oscilloscope. The result on the scope was that the pin did not toggle every time as expected, but it stay for one complete period low or high.

ACTIVE_LOW is 0.

0 Kudos
Reply

6,018 Views
falstaff
Senior Contributor I

Hi Johannes,

In the initial post you stated that it worked in Bash. So it does not work when using a loop in a bash script? How do you know whether it toggled the pin or whether it just had a glitch timewise (latency)? We recently used a Python script on one of our modules and got a pretty decent square wave, however we run it on a newer kernel.org Linux kernel:

http://developer.toradex.com/knowledge-base/python-in-linux

--

Stefan

0 Kudos
Reply

6,018 Views
johannestraxler
Contributor III

Hi Stefan,

in my initial post I mentioned that I just used the shell to check the status of the the GPIO file parallel to the C-Program. Let me explain again in detail:

1. Set GPIO to low in C-Program: write (gpio_fd, "0", 1);

2. Checked with scope: the pin is still HIGH!

3. Checked File-Status in shell: "cat /sys/class/gpio/gpio113/value" - returns "0", so even linux thinks that the pin is low, but it is actually high, because the scope doesn't lie! :smileywink:

4. Tried to explicitely set the pin to LOW: "echo 0 > /sys/class/gpio/gpio113/value" - suddenly the pin goes to LOW.

But this behaviour is not really reproducable, it happens stochastic.

In my second post I tried to set the GPIO from shell only and did this in a loop. Also here it happens, so it is not related to the C code.

I tried the loop with different intervals (100ms/500ms) which are quite long, so I could easily measure it with a scope.

0 Kudos
Reply

6,018 Views
falstaff
Senior Contributor I

Hi Johannes,

The reason the kernel does not see the value of the outside world is that the Input buffer is explicitly disabled in the old 3.0 kernel, when direction is "output":

http://git.toradex.com/cgit/linux-toradex.git/tree/arch/arm/plat-mxc/gpio-mvf.c?h=colibri_vf#n171

The driver upstream kernel driver explicitly does not change the input buffer, but leaves it up to the initial pinmux configuration whether the input buffer should be on or not (in our device trees we enable the input buffers for GPIO's):

http://git.toradex.com/cgit/linux-toradex.git/tree/drivers/pinctrl/freescale/pinctrl-imx.c?h=toradex...

However, this does not explain the stochastic behavior. Honestly, I currently don't know how why this happens.

--

Stefan

6,018 Views
johannestraxler
Contributor III

Dear Stefan,

thanks for your answer! Maybe I can modify the driver to be able to read the input buffer, so that I can set the output as long as the correct value is available, but this is just a workaround.

@Timesys Support: Can you check this issue and give feedback?


Thanks,

Johannes

0 Kudos
Reply

6,018 Views
timesyssupport
Senior Contributor II

Hello Johannes,

Our apologies for the delay in replying; our ping notifications have been silently bouncing on our end.

Our Vybrid kernel maintainers are reviewing, but as we have moved our Vybrid support to a 3.13 kernel, futher developments on the 3.0 kernel would need to be addressed as an engineering engagement.

Regards,

Timesys Support

6,018 Views
johannestraxler
Contributor III

Dear Timesys,

Unfortunately it is currently not possible to build a 3.13 Kernel for "PHYTEC phyCORE Vybrid Development Kit/pcm052" in your build factory. It is no problem for us to switch to a newer kernel!

Thanks,

Johannes

0 Kudos
Reply

6,018 Views
timesyssupport
Senior Contributor II

Hello Johannes,

We understand that Phytec is working to update their kernel support to the 3.13 release; until they have validated the kernel support, we will only be able to provide the 3.0 kernel. If you have a pressing need for this kernel release, we would suggest contacting Phytec to determine their roadmap.

Thank you,

Timesys Support

0 Kudos
Reply

6,018 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport  can you  share your comments about this case?

0 Kudos
Reply

6,018 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Timesys Support  do you have an update?

6,018 Views
karina_valencia
NXP Apps Support
NXP Apps Support

reminder

Timesys Support  do you have an update?

0 Kudos
Reply