Vybrid DMA inter-core collisions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid DMA inter-core collisions

Jump to solution
2,927 Views
kubiznak_petr
Contributor V

Two months ago, I described a DMA collision issue with Vybrid audio when a playback is started on Linux (A5) while MQX is running on M4 (Vybrid audio (sgtl5000)).

Now I am experiencing a mirror problem - when an SPI DMA operation starts on M4, Linux immediately dies. Is there any document describing which DMA channels are used by Timesys Linux so I can setup MQX to use different channels and avoid the issues? Can that be easily seen/modified in the Linux sources?

Labels (3)
0 Kudos
Reply
1 Solution
2,219 Views
timesyssupport
Senior Contributor II

Hello Petr,


On the Vybrid Tower board, Linux uses the following DMA channels on DMA engine 0, mux 0:

UART1 RX - Channel 4
UART1 TX - Channel 5

DSPI0 RX - Channel 12

DSPI0 TX - Channel 13


SAI2 (I2S2) RX - Channel 20
SAI2 (I2S2) TX - Channel 21

A list of all DMA channels can be found in the Linux source tree, at arch/arm/plat-mxc/include/mach/mvf_edma.h

Thanks, and let me know if you have any questions.

Timesys Support

View solution in original post

0 Kudos
Reply
5 Replies
2,220 Views
timesyssupport
Senior Contributor II

Hello Petr,


On the Vybrid Tower board, Linux uses the following DMA channels on DMA engine 0, mux 0:

UART1 RX - Channel 4
UART1 TX - Channel 5

DSPI0 RX - Channel 12

DSPI0 TX - Channel 13


SAI2 (I2S2) RX - Channel 20
SAI2 (I2S2) TX - Channel 21

A list of all DMA channels can be found in the Linux source tree, at arch/arm/plat-mxc/include/mach/mvf_edma.h

Thanks, and let me know if you have any questions.

Timesys Support

0 Kudos
Reply
2,218 Views
carlovalgocela
Contributor III

Hello timesyssupport

i would like to ask how in Linux the peripherals are assigned to DMA channels on DMA engine 0, mux 0?

0 Kudos
Reply
2,218 Views
timesyssupport
Senior Contributor II

Hello carlovalgocela

The following link should be helpful:

https://linuxlink.timesys.com/docs/wiki/engineering/bsp_userguide_twr-vf65gs10#DMA

Thank you,

Timesys Support

0 Kudos
Reply
2,218 Views
kubiznak_petr
Contributor V

Good, that should help, thank you.

0 Kudos
Reply
2,218 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 Kudos
Reply