Vybrid DMA inter-core collisions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid DMA inter-core collisions

跳至解决方案
2,884 次查看
kubiznak_petr
Contributor V

Two months ago, I described a DMA collision issue with Vybrid audio when a playback is started on Linux (A5) while MQX is running on M4 (Vybrid audio (sgtl5000)).

Now I am experiencing a mirror problem - when an SPI DMA operation starts on M4, Linux immediately dies. Is there any document describing which DMA channels are used by Timesys Linux so I can setup MQX to use different channels and avoid the issues? Can that be easily seen/modified in the Linux sources?

标签 (3)
0 项奖励
回复
1 解答
2,176 次查看
timesyssupport
Senior Contributor II

Hello Petr,


On the Vybrid Tower board, Linux uses the following DMA channels on DMA engine 0, mux 0:

UART1 RX - Channel 4
UART1 TX - Channel 5

DSPI0 RX - Channel 12

DSPI0 TX - Channel 13


SAI2 (I2S2) RX - Channel 20
SAI2 (I2S2) TX - Channel 21

A list of all DMA channels can be found in the Linux source tree, at arch/arm/plat-mxc/include/mach/mvf_edma.h

Thanks, and let me know if you have any questions.

Timesys Support

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,177 次查看
timesyssupport
Senior Contributor II

Hello Petr,


On the Vybrid Tower board, Linux uses the following DMA channels on DMA engine 0, mux 0:

UART1 RX - Channel 4
UART1 TX - Channel 5

DSPI0 RX - Channel 12

DSPI0 TX - Channel 13


SAI2 (I2S2) RX - Channel 20
SAI2 (I2S2) TX - Channel 21

A list of all DMA channels can be found in the Linux source tree, at arch/arm/plat-mxc/include/mach/mvf_edma.h

Thanks, and let me know if you have any questions.

Timesys Support

0 项奖励
回复
2,175 次查看
carlovalgocela
Contributor III

Hello timesyssupport

i would like to ask how in Linux the peripherals are assigned to DMA channels on DMA engine 0, mux 0?

0 项奖励
回复
2,175 次查看
timesyssupport
Senior Contributor II

Hello carlovalgocela

The following link should be helpful:

https://linuxlink.timesys.com/docs/wiki/engineering/bsp_userguide_twr-vf65gs10#DMA

Thank you,

Timesys Support

0 项奖励
回复
2,175 次查看
kubiznak_petr
Contributor V

Good, that should help, thank you.

0 项奖励
回复
2,175 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 项奖励
回复