Vybrid DMA Request from GPIO Input

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid DMA Request from GPIO Input

跳至解决方案
2,938 次查看
nathanb_
Contributor III

Hello All,

I'm currently trying to trigger a DMA request from an external GPIO input (PORT2[2]).

I can mux the GPIO input, and set the PCR->IRQC to 0xA and I get an interrupt generated no problem.

However, when I set the PCR->IRQC to 0x2, I never get a DMA request signal from DMA request source 41.

If I change the DMA request source to 24 (a flextimer I currently have running in DMA mode ), the DMA works correctly.

Does anyone know what's going on here?  Can anyone confirm that DMA requests from GPIO inputs correctly function?

Thanks.

标签 (6)
标记 (3)
0 项奖励
回复
1 解答
2,562 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

It is not stated in the documentation but according to my tests it seems that the Table 3-2 is not correct.

The PORTA -PORTE should be PORT0-PORT4. With that modification the Table 3-31 matches and corresponds to the behavior you are facing.

As you can see PORT2[2] corresponds to PTD28 but at the end it belongs to PORT2 and DMA source 40 corresponds.

Best Regards,

Alejandro

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,562 次查看
nathanb_
Contributor III

Oddly enough, I changed the request source to 40 and now it works.

However, PORT2[2] is PTD28.

Source 40 is PORT C in the manual.

Any clarity?

0 项奖励
回复
2,563 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

It is not stated in the documentation but according to my tests it seems that the Table 3-2 is not correct.

The PORTA -PORTE should be PORT0-PORT4. With that modification the Table 3-31 matches and corresponds to the behavior you are facing.

As you can see PORT2[2] corresponds to PTD28 but at the end it belongs to PORT2 and DMA source 40 corresponds.

Best Regards,

Alejandro

0 项奖励
回复
2,562 次查看
nathanb_
Contributor III

Thanks Alejandro,

This is what I was suspecting when I tried 40.

0 项奖励
回复