Video input couplling capacitance valu.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Video input couplling capacitance valu.

ソリューションへジャンプ
1,681件の閲覧回数
takashitakahash
Contributor III

Dear community.
Descriptione on VYBRIDRSERIESEC Rev 7,11/2014 of  P43 9.1.3 VideoADC Specifications.

The  External AC coupling max spec is 47nF.

But ref evaluation board with a 0.1uF. It is beyond the specs, Is it mistake described CEC or  need to increase in noise measures.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,498件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I just checked at the spec in the datasheet. And the 47nF refer to the typical vaule not the maximum value.

/Alejandro

元の投稿で解決策を見る

1 返信
1,499件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I just checked at the spec in the datasheet. And the 47nF refer to the typical vaule not the maximum value.

/Alejandro