Video input couplling capacitance valu.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Video input couplling capacitance valu.

Jump to solution
1,680 Views
takashitakahash
Contributor III

Dear community.
Descriptione on VYBRIDRSERIESEC Rev 7,11/2014 of  P43 9.1.3 VideoADC Specifications.

The  External AC coupling max spec is 47nF.

But ref evaluation board with a 0.1uF. It is beyond the specs, Is it mistake described CEC or  need to increase in noise measures.

Labels (1)
0 Kudos
Reply
1 Solution
1,497 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I just checked at the spec in the datasheet. And the 47nF refer to the typical vaule not the maximum value.

/Alejandro

View solution in original post

1 Reply
1,498 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I just checked at the spec in the datasheet. And the 47nF refer to the typical vaule not the maximum value.

/Alejandro