Video input couplling capacitance valu.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Video input couplling capacitance valu.

跳至解决方案
1,679 次查看
takashitakahash
Contributor III

Dear community.
Descriptione on VYBRIDRSERIESEC Rev 7,11/2014 of  P43 9.1.3 VideoADC Specifications.

The  External AC coupling max spec is 47nF.

But ref evaluation board with a 0.1uF. It is beyond the specs, Is it mistake described CEC or  need to increase in noise measures.

标签 (1)
0 项奖励
回复
1 解答
1,496 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I just checked at the spec in the datasheet. And the 47nF refer to the typical vaule not the maximum value.

/Alejandro

在原帖中查看解决方案

1 回复
1,497 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I just checked at the spec in the datasheet. And the 47nF refer to the typical vaule not the maximum value.

/Alejandro