VF6xx linux VIU driver (v4l)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VF6xx linux VIU driver (v4l)

ソリューションへジャンプ
2,765件の閲覧回数
josa
Contributor II

Hi

I have a VF6x based board (toradex vf61) and i would like to use the Analog video inputs for video capture using the v4l core.

Is there any soc driver for the VF6x available that supports the VIU system?

Any help appreciated.

Johan

ラベル(2)
0 件の賞賛
返信
1 解決策
2,377件の閲覧回数
timesyssupport
Senior Contributor II

Hello,

We currently do not have the toradex vf61 board. For the Vybrid Tower, we do not have a video input driver available in the Linux kernel - it is not on our roadmap at this time either, as it is not broken out in a useful manner and conflicts with too many other peripherals. If you are looking for assistance with driver development, Timesys can help under a professional services agreement - please contact [email protected] for more information.

Thanks,

Timesys Support

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,378件の閲覧回数
timesyssupport
Senior Contributor II

Hello,

We currently do not have the toradex vf61 board. For the Vybrid Tower, we do not have a video input driver available in the Linux kernel - it is not on our roadmap at this time either, as it is not broken out in a useful manner and conflicts with too many other peripherals. If you are looking for assistance with driver development, Timesys can help under a professional services agreement - please contact [email protected] for more information.

Thanks,

Timesys Support

0 件の賞賛
返信
2,377件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 件の賞賛
返信