VF6xx linux VIU driver (v4l)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

VF6xx linux VIU driver (v4l)

跳至解决方案
2,772 次查看
josa
Contributor II

Hi

I have a VF6x based board (toradex vf61) and i would like to use the Analog video inputs for video capture using the v4l core.

Is there any soc driver for the VF6x available that supports the VIU system?

Any help appreciated.

Johan

标签 (2)
0 项奖励
回复
1 解答
2,384 次查看
timesyssupport
Senior Contributor II

Hello,

We currently do not have the toradex vf61 board. For the Vybrid Tower, we do not have a video input driver available in the Linux kernel - it is not on our roadmap at this time either, as it is not broken out in a useful manner and conflicts with too many other peripherals. If you are looking for assistance with driver development, Timesys can help under a professional services agreement - please contact [email protected] for more information.

Thanks,

Timesys Support

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,385 次查看
timesyssupport
Senior Contributor II

Hello,

We currently do not have the toradex vf61 board. For the Vybrid Tower, we do not have a video input driver available in the Linux kernel - it is not on our roadmap at this time either, as it is not broken out in a useful manner and conflicts with too many other peripherals. If you are looking for assistance with driver development, Timesys can help under a professional services agreement - please contact [email protected] for more information.

Thanks,

Timesys Support

0 项奖励
回复
2,384 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 项奖励
回复