VF6xx linux VIU driver (v4l)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VF6xx linux VIU driver (v4l)

Jump to solution
2,144 Views
josa
Contributor II

Hi

I have a VF6x based board (toradex vf61) and i would like to use the Analog video inputs for video capture using the v4l core.

Is there any soc driver for the VF6x available that supports the VIU system?

Any help appreciated.

Johan

Labels (2)
0 Kudos
Reply
1 Solution
1,756 Views
timesyssupport
Senior Contributor II

Hello,

We currently do not have the toradex vf61 board. For the Vybrid Tower, we do not have a video input driver available in the Linux kernel - it is not on our roadmap at this time either, as it is not broken out in a useful manner and conflicts with too many other peripherals. If you are looking for assistance with driver development, Timesys can help under a professional services agreement - please contact sales@timesys.com for more information.

Thanks,

Timesys Support

View solution in original post

0 Kudos
Reply
2 Replies
1,757 Views
timesyssupport
Senior Contributor II

Hello,

We currently do not have the toradex vf61 board. For the Vybrid Tower, we do not have a video input driver available in the Linux kernel - it is not on our roadmap at this time either, as it is not broken out in a useful manner and conflicts with too many other peripherals. If you are looking for assistance with driver development, Timesys can help under a professional services agreement - please contact sales@timesys.com for more information.

Thanks,

Timesys Support

0 Kudos
Reply
1,756 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 Kudos
Reply