VF6xx VYBRID Cortex-M4 Cache sample code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VF6xx VYBRID Cortex-M4 Cache sample code

ソリューションへジャンプ
4,684件の閲覧回数
wushengjiang
Contributor II

Is there any sample for VF6xx VYBRID Cortex-M4 cache operation?

It seems data cache operation is not success when debug with network on Cortext-M4, network packet loss when data cache is on, after disable data cache on Cortex-M4, no packet loss.

The same code works well on Cortex-A5 side which has PL310 L2 cache.

タグ(2)
0 件の賞賛
返信
1 解決策
4,411件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,412件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
4,412件の閲覧回数
timesyssupport
Senior Contributor II

Hello Wu,

Presumably you are working with MQX in this case? There is the following, which tests some cache operations: mqx/examples/benchmrk/codesize/main.c

karinavalencia​ - if this is MQX, can the MQX team review?

Thank you,

Timesys Support

0 件の賞賛
返信
4,412件の閲覧回数
wushengjiang
Contributor II

Thanks for all your help, I found the cache.c under folder mqx\source\psp\cortex_m, I will compare it with current driver.

0 件の賞賛
返信
4,412件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Lets wait the update from Wu.

0 件の賞賛
返信
4,412件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ an you help here?

0 件の賞賛
返信