VF6xx VYBRID Cortex-M4 Cache sample code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VF6xx VYBRID Cortex-M4 Cache sample code

Jump to solution
4,855 Views
wushengjiang
Contributor II

Is there any sample for VF6xx VYBRID Cortex-M4 cache operation?

It seems data cache operation is not success when debug with network on Cortext-M4, network packet loss when data cache is on, after disable data cache on Cortex-M4, no packet loss.

The same code works well on Cortex-A5 side which has PL310 L2 cache.

Tags (2)
0 Kudos
Reply
1 Solution
4,582 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
5 Replies
4,583 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
4,583 Views
timesyssupport
Senior Contributor II

Hello Wu,

Presumably you are working with MQX in this case? There is the following, which tests some cache operations: mqx/examples/benchmrk/codesize/main.c

karinavalencia​ - if this is MQX, can the MQX team review?

Thank you,

Timesys Support

0 Kudos
Reply
4,583 Views
wushengjiang
Contributor II

Thanks for all your help, I found the cache.c under folder mqx\source\psp\cortex_m, I will compare it with current driver.

0 Kudos
Reply
4,583 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Lets wait the update from Wu.

0 Kudos
Reply
4,583 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ an you help here?

0 Kudos
Reply