VF61 Linux SPI DMA support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

VF61 Linux SPI DMA support

跳至解决方案
3,967 次查看
olegpetrakivsky
Contributor I

spi-fsl-dspi driver does not supports DMA. I made some driver modification for DMA support.

After code test I got next result. DMA transmit is ok. DMA receives about 50% of lost packets (some parts of buffer contents previous message). The issue is in DMA. Not all data are copied from device fifo into memory. RXCTR = 0 in rx callback transaction indicates that data is read. SPIx_RXFRn register shows a new correct value. Do you have idea about reason of bad DMA transfers? Draft code is attached.

Original Attachment has been moved to: spi-fsl-dspi.c.zip

标签 (1)
0 项奖励
回复
1 解答
3,565 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,566 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
3,566 次查看
timesyssupport
Senior Contributor II

Hi Oleg Petrakivskyi,

Apologies for our delayed response.

From your information, DMA transmission is fine. Overall domination among the bus is changed into the interrupt controller after the CPU acknowledges DMA request, to verify Rx FIFO - could you please share your slave peripheral device hardware information with us. It'll help us to debug/reproduce your issue in my end.

Thanks

Timesys Support

3,566 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Timesys Support do you have an update?

0 项奖励
回复
3,566 次查看
olegpetrakivsky
Contributor I
3,566 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help here?

0 项奖励
回复