VF5xx / support DDR2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,111件の閲覧回数
soichiyamamoto
Contributor V

Hello

Dose VF5xx support DDR2 ?

Best regards,

soichi.yamamoto

タグ(2)
0 件の賞賛
返信
1 解決策
2,011件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Soichi,

No, it does not:

  1. The Datasheet states "16 bit DRAM Controller with support for LPDDR2/DDR3 - Up to 400 MHz (ECC supported)".
  2. According to the Datasheet, table "Recommended Operating conditions", voltage values for the   SDRAMC_VDD1P5 power rails are either 1.2V (LPDDR2) or 1.5V (DDR3), not 1.8V required for DDR2.

Sincerely yours, Naoum Gitnik.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,012件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Soichi,

No, it does not:

  1. The Datasheet states "16 bit DRAM Controller with support for LPDDR2/DDR3 - Up to 400 MHz (ECC supported)".
  2. According to the Datasheet, table "Recommended Operating conditions", voltage values for the   SDRAMC_VDD1P5 power rails are either 1.2V (LPDDR2) or 1.5V (DDR3), not 1.8V required for DDR2.

Sincerely yours, Naoum Gitnik.

0 件の賞賛
返信
2,011件の閲覧回数
soichiyamamoto
Contributor V

Dear Naoum,

Thank you very much for your help.

Best Regards,

soichi yamamoto,

0 件の賞賛
返信