VF5xx / support DDR2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VF5xx / support DDR2

Jump to solution
2,175 Views
soichiyamamoto
Contributor V

Hello

Dose VF5xx support DDR2 ?

Best regards,

soichi.yamamoto

Tags (2)
0 Kudos
Reply
1 Solution
2,075 Views
naoumgitnik
Senior Contributor V

Dear Soichi,

No, it does not:

  1. The Datasheet states "16 bit DRAM Controller with support for LPDDR2/DDR3 - Up to 400 MHz (ECC supported)".
  2. According to the Datasheet, table "Recommended Operating conditions", voltage values for the   SDRAMC_VDD1P5 power rails are either 1.2V (LPDDR2) or 1.5V (DDR3), not 1.8V required for DDR2.

Sincerely yours, Naoum Gitnik.

View solution in original post

0 Kudos
Reply
2 Replies
2,076 Views
naoumgitnik
Senior Contributor V

Dear Soichi,

No, it does not:

  1. The Datasheet states "16 bit DRAM Controller with support for LPDDR2/DDR3 - Up to 400 MHz (ECC supported)".
  2. According to the Datasheet, table "Recommended Operating conditions", voltage values for the   SDRAMC_VDD1P5 power rails are either 1.2V (LPDDR2) or 1.5V (DDR3), not 1.8V required for DDR2.

Sincerely yours, Naoum Gitnik.

0 Kudos
Reply
2,075 Views
soichiyamamoto
Contributor V

Dear Naoum,

Thank you very much for your help.

Best Regards,

soichi yamamoto,

0 Kudos
Reply