Using OpenVG with 2D ACE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using OpenVG with 2D ACE?

跳至解决方案
2,106 次查看
johnhom
Contributor III

Hello.

When using using OpenVG on Vybrid, can we route the output to a memory-mapped frame buffer and feed that as a layer into the 2D ACE, making use of its composition capabilities and layers? Or is it that the OpenVG output always outputs to the display?

标记 (3)
1 解答
1,800 次查看
johnhom
Contributor III

Thanks for the suggestion for moving the post. I thought I had opened it in the Vybrid Processors Community Place, but anyway I've moved it now.

My colleague has answered my question, and the answer is yes, the OpenVG output can be used as an input to the 2D ACE for composition with other layers.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,800 次查看
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Vybrid Processors ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community. 

0 项奖励
回复
1,801 次查看
johnhom
Contributor III

Thanks for the suggestion for moving the post. I thought I had opened it in the Vybrid Processors Community Place, but anyway I've moved it now.

My colleague has answered my question, and the answer is yes, the OpenVG output can be used as an input to the 2D ACE for composition with other layers.

0 项奖励
回复