Using OpenVG with 2D ACE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using OpenVG with 2D ACE?

ソリューションへジャンプ
2,166件の閲覧回数
johnhom
Contributor III

Hello.

When using using OpenVG on Vybrid, can we route the output to a memory-mapped frame buffer and feed that as a layer into the 2D ACE, making use of its composition capabilities and layers? Or is it that the OpenVG output always outputs to the display?

タグ(3)
1 解決策
1,860件の閲覧回数
johnhom
Contributor III

Thanks for the suggestion for moving the post. I thought I had opened it in the Vybrid Processors Community Place, but anyway I've moved it now.

My colleague has answered my question, and the answer is yes, the OpenVG output can be used as an input to the 2D ACE for composition with other layers.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,860件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Vybrid Processors ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community. 

0 件の賞賛
返信
1,861件の閲覧回数
johnhom
Contributor III

Thanks for the suggestion for moving the post. I thought I had opened it in the Vybrid Processors Community Place, but anyway I've moved it now.

My colleague has answered my question, and the answer is yes, the OpenVG output can be used as an input to the 2D ACE for composition with other layers.

0 件の賞賛
返信