Hello ,
I am using Vf5xxR series board. I want to boot it from sdcard. I have done following jumper setting on the board.
In order to boot from the SD interface, the following switches must be turned ON. The
RCON bits switches must be set ON is in the up position.
o [SW10] -5, 6
o [SW11] - 11
o Jumper J15 is on pins 2 and 3
At the offset of 1k i have flashed my uboot.
I have connected the board to Linux-PC with a 9-pin RS232 cable and started mini-com.(/dev/ttyUSB0)
But I am not able to get the u-boot console.Do I am missing some jumper settings.Or i am missing some steps for sdcard boot.
Thanks,
Shrikant