USB analog registers missing in reference manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB analog registers missing in reference manual

Jump to solution
2,434 Views
markwatson
Contributor III

The following registers are missing in the Rev. 7 manual:

USB_ANALOG_USB0_VBUS_DETECT

USB_ANALOG_USB0_CHRG_DETECT

USB_ANALOG_USB0_MISC

and the corresponding ones for the USB1 channel. 

Help. I need this information.

Labels (1)
0 Kudos
Reply
1 Solution
2,244 Views
richard_stulens
NXP Employee
NXP Employee

Mark,

That is correct. The sections were incidentally shipped during the generation of the release copy.

We are currently preparing a new revision of the RM in which this issue will be resolved.

I have attached the USB analog chapter from our internal review copy. All information should be there.

Best regards,

Richard

View solution in original post

0 Kudos
Reply
2 Replies
2,245 Views
richard_stulens
NXP Employee
NXP Employee

Mark,

That is correct. The sections were incidentally shipped during the generation of the release copy.

We are currently preparing a new revision of the RM in which this issue will be resolved.

I have attached the USB analog chapter from our internal review copy. All information should be there.

Best regards,

Richard

0 Kudos
Reply
2,244 Views
markwatson
Contributor III

Richard,

Thank you very much. This information will allow me to get our USB connect/disconnect sensing working correctly.

Best regards,

Mark

0 Kudos
Reply