USB analog registers missing in reference manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB analog registers missing in reference manual

ソリューションへジャンプ
3,388件の閲覧回数
markwatson
Contributor III

The following registers are missing in the Rev. 7 manual:

USB_ANALOG_USB0_VBUS_DETECT

USB_ANALOG_USB0_CHRG_DETECT

USB_ANALOG_USB0_MISC

and the corresponding ones for the USB1 channel. 

Help. I need this information.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,198件の閲覧回数
richard_stulens
NXP Employee
NXP Employee

Mark,

That is correct. The sections were incidentally shipped during the generation of the release copy.

We are currently preparing a new revision of the RM in which this issue will be resolved.

I have attached the USB analog chapter from our internal review copy. All information should be there.

Best regards,

Richard

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,199件の閲覧回数
richard_stulens
NXP Employee
NXP Employee

Mark,

That is correct. The sections were incidentally shipped during the generation of the release copy.

We are currently preparing a new revision of the RM in which this issue will be resolved.

I have attached the USB analog chapter from our internal review copy. All information should be there.

Best regards,

Richard

0 件の賞賛
返信
3,198件の閲覧回数
markwatson
Contributor III

Richard,

Thank you very much. This information will allow me to get our USB connect/disconnect sensing working correctly.

Best regards,

Mark

0 件の賞賛
返信