Software Difference

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,188件の閲覧回数
keisukewatanabe
Contributor III

Dear support,

Is/are there difference(s) between the (Freescale Provided) basic software libraries of VF5 and VF6?

The point of this question is that we are developing our software based on the VF6 evaluation board,

and we are anxious if the software can work on our final target board which will be build on VF5.

Best regards,

Keisuke

ラベル(3)
1 解決策
1,996件の閲覧回数
Jmart
NXP Employee
NXP Employee

Keisuke,

The main difference between the VF5 and VF6 Vybrid silicon is the addition of the Cortex-M4 core to the VF6. As long as your software does not utilize the Cortex-M4, you can expect your application code to run the same when you move to your target hardware.

All the best.

元の投稿で解決策を見る

1 返信
1,997件の閲覧回数
Jmart
NXP Employee
NXP Employee

Keisuke,

The main difference between the VF5 and VF6 Vybrid silicon is the addition of the Cortex-M4 core to the VF6. As long as your software does not utilize the Cortex-M4, you can expect your application code to run the same when you move to your target hardware.

All the best.