SDHC errata

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,501件の閲覧回数
makotokatsukura
Contributor II

Dear forum members,

    My team is making a product using Vybrid VF5 and Linux 3.0 ( provided
by Timesys ). We use a multi media card (SD-CARD) to store our customers’ data.
However, we found that there are some errata around SDHC function of Vybrid.

Errata around SDHC are as follows:

 

  1. e3980 “SDHC: Glitch is generated on card clock with software reset
    or clock divider change”
  2. e3981 “SDHC: ADMA fails when data length in the last descriptor is
    less or equal to 4 bytes”
  3. e3982 “SDHC: ADMA transfer error when the block size is not a
    multiple of four”
  4. e3983 “SDHC: Problem when ADMA2 last descriptor is LINK or NOP”
  5. e4627 “SDHC: Erroneous CMD CRC error and CMD Index error may occur
    on sending new CMD during data transfer”

            

I just want to know that Linux SDHC drivers in Timesys Linux are already modified to avoid those errata or not.
If not, we need to plan to modify the code to avoid those errata.

    

Best regards,

Makoto Katsukura

Referense:

  Vybrid Errata ( Vybrid 1N02G )

http://cache.freescale.com/files/32bit/doc/errata/VYBRID_1N02G.pdf

ラベル(3)
0 件の賞賛
返信
1 解決策
2,032件の閲覧回数
timesyssupport
Senior Contributor II

Hello Katsukura-san,

As far as I am aware, these errata have not been addressed in the Linux 3.0 kernel for Vybrid. Please let me know if you have any additional questions.

Thanks,

Timesys Support

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,033件の閲覧回数
timesyssupport
Senior Contributor II

Hello Katsukura-san,

As far as I am aware, these errata have not been addressed in the Linux 3.0 kernel for Vybrid. Please let me know if you have any additional questions.

Thanks,

Timesys Support

0 件の賞賛
返信
2,032件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help on this case?

0 件の賞賛
返信