RTIC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
10,842 Views
东升王
Contributor II

Hi

I am working on Vybrid platform to enable RTIC feature. When I wrote those registers, the value I read back was always zero. Even I used U-boot. For example:

I wrote : CAAM_RTIC_BASE_PTR->RWDOG = 0xffff;

              CAAM_RTIC_BASE_PTR->RTHR = 0x1;

Then the value I read back was :

              CAAM_RTIC_BASE_PTR->RWDOG = 0x0;

              CAAM_RTIC_BASE_PTR->RTHR = 0x0;

Somebody can tell me why?

Thank you

1 Solution
9,425 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
14 Replies
9,426 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
9,426 Views
karina_valencia
NXP Apps Support
NXP Apps Support

东升王​  did you send Rene  the information requested?

0 Kudos
Reply
9,426 Views
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ FYI

0 Kudos
Reply
9,426 Views
karina_valencia
NXP Apps Support
NXP Apps Support

dongshengwang​ did you get previous comment?

0 Kudos
Reply
9,423 Views
东升王
Contributor II

Hi Karinavalencia

Sorry I just got your email. Here is my code for rtic. Thanks for your

help.

Regards,

Dongsheng Wang

0 Kudos
Reply
9,423 Views
rendy
NXP Employee
NXP Employee

Hello,

please send me *working* example - send me the project with all headers and sources needed.

Thanks
Rene

9,423 Views
rendy
NXP Employee
NXP Employee

Hello,

please send me a short example which demonstrates this and I will check it soon. You can use TWR-VF65GS10 sample code.

Thanks

Rene

9,423 Views
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ do you have an update?

0 Kudos
Reply
9,423 Views
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ can you share your comments?

0 Kudos
Reply
9,423 Views
东升王
Contributor II

Sure, no problem!

0 Kudos
Reply
9,423 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help to review this case?

0 Kudos
Reply
9,423 Views
timesyssupport
Senior Contributor II

Hello Dongsheng,

Ensure that, RTIC is not in Run-time mode before writing to those registers as they are read only while in Run-time mode. Use RSTA register to find out the state of RTIC.

Thanks,

Timesys Support

0 Kudos
Reply
9,423 Views
东升王
Contributor II

Hi

Yes, before I wrote these registers. I checked RSTA register. It is always zero. Actually every registers are always zero. Even I read and wrote them with U-boot.

Thank you

0 Kudos
Reply
9,423 Views
timesyssupport
Senior Contributor II

Hi,

RTIC registers are set with 0 by default.I referred VYBRIDSRM and don't have much information to share. karinavalencia Can you ask the NXP Vybrid team to comment with any other information?

Thanks,

Timesys Support

0 Kudos
Reply