RTIC Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,705件の閲覧回数
东升王
Contributor II

Hi

I am now developing rtic feature on Vybrid 610 platform. From the security_manual. It mentions "

Due to timing issues, instead of polling this register (RSTA) software should read the RTIC Status

Register after an RTIC done interrupt."

My question is where I can get the irq. From caam irq? All submodules of caam share the same irq? I can not find that detail from manual.

Thank you

0 件の賞賛
返信
1 解決策
3,452件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,453件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
3,452件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Service Request (SR).

How to submit a new question for NXP Support

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信