Question on AC97 interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question on AC97 interface

ソリューションへジャンプ
2,401件の閲覧回数
DanKSI
Contributor III

Hi.

I am looking to connect a Wolfson WM9712 audio codec, which uses the AC97 AC-Link connection, to the Vybrid processor's SAI peripheral.  I have not used this interface before, but I've put together my best guess on what the pin connections should be.

(Vybrid) SAI_TX_DATA -> SDATAOUT (Wolfson)

(Vybrid) SAI_RX_BCLK <- BITCLK (Wolfson)

(Vybrid) SAI_RX_DATA <- SDATAIN (Wolfson)

(Vybrid) SAI_TX_SYNC -> SYNC (Wolfson)

(Vybrid) Any I/O -> RESETB (Wolfson)

Any help verifying this pinout would be great.

Thanks,

Dan

タグ(3)
0 件の賞賛
返信
1 解決策
2,173件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,174件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
2,173件の閲覧回数
VilemZ
NXP Employee
NXP Employee

Hi Dan,

It seems be OK.

Best regards

Vilem

0 件の賞賛
返信
2,173件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Vilem,

Thanks for verifying the connections, this will help me too.

Regards,

Alejandro

0 件の賞賛
返信