Question on AC97 interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question on AC97 interface

Jump to solution
2,599 Views
DanKSI
Contributor III

Hi.

I am looking to connect a Wolfson WM9712 audio codec, which uses the AC97 AC-Link connection, to the Vybrid processor's SAI peripheral.  I have not used this interface before, but I've put together my best guess on what the pin connections should be.

(Vybrid) SAI_TX_DATA -> SDATAOUT (Wolfson)

(Vybrid) SAI_RX_BCLK <- BITCLK (Wolfson)

(Vybrid) SAI_RX_DATA <- SDATAIN (Wolfson)

(Vybrid) SAI_TX_SYNC -> SYNC (Wolfson)

(Vybrid) Any I/O -> RESETB (Wolfson)

Any help verifying this pinout would be great.

Thanks,

Dan

Tags (3)
0 Kudos
Reply
1 Solution
2,371 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
3 Replies
2,372 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
2,371 Views
VilemZ
NXP Employee
NXP Employee

Hi Dan,

It seems be OK.

Best regards

Vilem

0 Kudos
Reply
2,371 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Vilem,

Thanks for verifying the connections, this will help me too.

Regards,

Alejandro

0 Kudos
Reply