Qt 4.8 embedded - multitouch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Qt 4.8 embedded - multitouch

Jump to solution
7,009 Views
davidw_
Contributor II

We are currently developing a graphical Qt application for an embedded system with Vybrid vf610 and we have a hard time trying to get Qt multitouch working.
Our setup is:
Qt (embedded) 4.8.5 with QWS server
Linux -  Timesys build for Vybrid vf610 with 3.13 kernel
Touchscreen driver: edt-ft5x06 (upstream version)

We managed to get touchscreen working in Qt using Tslib or LinuxInput drivers, but it registers just one finger at a time and the Qt application only receives mouse events, not touch events or gestures.
The kernel drivers seem to be working properly, touchscreen shows up as /dev/input/eventX and sends proper events of what seems to be Linux multitouch protocol B (see evtest.dump attachment)

For touchscreen testing, we have tried the tslib software (both version 1.0 with Timesys multitouch patch and version 1.1, which should support multitouch by itself). However, the inbuilt tslib test applications (ts_test, ts_print) don't seem to support multitouch by design. Single touch works properly.

In Qt, we have tried several touch, multitouch and gesture examples, but none work with more than one finger. From the source code it seems that none of the mouse drivers for QWS (qmouselinuxinput_qws.cpp, qmouselinuxtp_qws.cpp, qmousetslib_qws.cpp) support sending Qt touch events and there is no dedicated touch driver. Only the generic qlinuxinput.cpp mouse driver plugin seems to support Qt touch events using #define QT_QPA_EXPERIMENTAL_TOUCHEVENT, but doesn't seem to be available for use with QWS anyway.

Is there something what could be done that we are missing? It seems strange that there is documentation about using gestures in Qt and examples but no support for multitouch in drivers. The Internet doesn't offer many clues other than this:
http://www.ptrackapp.com/apclassys-notes/embedded-linux-multitouch/
ant that doesn't look like a proper solution.

Attachments:
evtest.dump - events from kernel touchscreen drivers
qlinuxinput.cpp - LinuxInput driver with experimental Qt touch support. Not available (?) for QWS
qmouselinuxinput_qws.cpp - LinuxInput driver for QWS, no Qt touch event support
qmousetslib_qws.cpp - Tslib driver for QWS, no Qt touch event support

Original Attachment has been moved to: qmouselinuxinput_qws.cpp.zip

Original Attachment has been moved to: evtest.dump.zip

Original Attachment has been moved to: qlinuxinput.cpp.zip

Original Attachment has been moved to: qmousetslib_qws.cpp.zip

1 Solution
4,885 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
12 Replies
4,886 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
4,892 Views
rendy
NXP Employee
NXP Employee

Hi,

what's your HW setup? Can you replicate the issue on Freescale HW, e.g. on Vybrid tower board?

Regards

Rene

0 Kudos
Reply
4,892 Views
karina_valencia
NXP Apps Support
NXP Apps Support

davidw.​ did you get previous comment?

0 Kudos
Reply
4,892 Views
davidw_
Contributor II

karinavalencia: No, I didn't notice, thank you for letting me know.

rendy: The hardware is custom made with main components based on the Vybrid Tower, however the display is completely different (Glyn ETMV570G0BDHU with Focaltech FT5406 touchscreen controller). AFAIK the tower board display's driver crtouch_ts doesn't offer multitouch functionality (looks like a work in progress), so the issue can't be replicated on Vybrid tower. But thank you for offering your help.

For reference: I exchanged some emails with Timesys and they recommend moving to Qt5, because it should offer much better multitouch support. Multitouch in Qt4 is "quite incomplete" and requires "a number of manual steps", as described in the ptrackapp.com link in my original post, to start working.

So for now I have to focus on other issues. We have not yet decided whether to move to Qt5 or try to implement multitouch in Qt4.

0 Kudos
Reply
4,892 Views
timesyssupport
Senior Contributor II

Hi David,

Allow us some time to review; we've been investigating multi-touch in Qt 5 and it's functionality with tslib. We haven't visited Qt 4.8 with regards to multi-touch yet, but will investigate and report back.

Thank you,

Timesys Support

0 Kudos
Reply
4,892 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ do you have an update?

0 Kudos
Reply
4,892 Views
timesyssupport
Senior Contributor II

Hello,

Not at this time - investigating currently. Qt5 relies on mtdev to provide multi-touch support; that was a later addition, which the 4.8.x series may not have received. karinavalencia​ is there not a Qt developer who can be of assistance here to clarify/confirm multi-touch availability in Qt 4.8.x?

Regards,

Timesys Support

0 Kudos
Reply
4,892 Views
rendy
NXP Employee
NXP Employee

Hi,

I can assist, however we haven't any multitouch display available here.

Regards

Rene

4,892 Views
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ are you able to help here?

0 Kudos
Reply
4,892 Views
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ do you have an update?

0 Kudos
Reply
4,892 Views
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ your action is required to provide an update ASAP.

PSA​ FYI

0 Kudos
Reply
4,892 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help with this case?

0 Kudos
Reply