Pin termination DDR address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin termination DDR address

Jump to solution
1,885 Views
keisukewatanabe
Contributor III

Dear support,

We are planning to use DDR with 14bit address input.

Please teach us how to terminate unused address bits of Vybrid (DDR_A[14] and DDR_A[15]).

In the reference circuit, unused address bit was connected to VTT_DDR3 via 47ohm resister.

Best regards,

Keisuke

Labels (1)
0 Kudos
Reply
1 Solution
1,721 Views
naoumgitnik
Senior Contributor V

Dear Keisuke,

You may use the same approach as the reference circuit does.

At the same time, termination is required for impedance matching of a toggling line, but unused lines do not toggle...

Best regards, Naoum Gitnik.

View solution in original post

0 Kudos
Reply
1 Reply
1,722 Views
naoumgitnik
Senior Contributor V

Dear Keisuke,

You may use the same approach as the reference circuit does.

At the same time, termination is required for impedance matching of a toggling line, but unused lines do not toggle...

Best regards, Naoum Gitnik.

0 Kudos
Reply