PTB18 & PTB19

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,348件の閲覧回数
xueweiliu
Contributor I

The latest Version of Vybrid is 1.1, I believe that the Errata for 1.0 "System: Pins PTB18 and PTB19 need to be driven at boot." has been fixed, right?

And should I need to drive these two pins when boot from RCON mode on the Vybrid 1.1 chip?

Are there some things should I pay attention to when use the two ports as GPIO or alternative function?

Thanks,

Xuewei

タグ(2)
0 件の賞賛
返信
1 解決策
3,176件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Yes, there is no longer a need to drive those pins on 1.1. They can be treated like any other GPIO.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,176件の閲覧回数
xueweiliu
Contributor I

Thanks!

0 件の賞賛
返信
3,177件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Yes, there is no longer a need to drive those pins on 1.1. They can be treated like any other GPIO.

0 件の賞賛
返信