PTB18 & PTB19

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PTB18 & PTB19

跳至解决方案
3,403 次查看
xueweiliu
Contributor I

The latest Version of Vybrid is 1.1, I believe that the Errata for 1.0 "System: Pins PTB18 and PTB19 need to be driven at boot." has been fixed, right?

And should I need to drive these two pins when boot from RCON mode on the Vybrid 1.1 chip?

Are there some things should I pay attention to when use the two ports as GPIO or alternative function?

Thanks,

Xuewei

标记 (2)
0 项奖励
回复
1 解答
3,231 次查看
anthony_huereca
NXP Employee
NXP Employee

Yes, there is no longer a need to drive those pins on 1.1. They can be treated like any other GPIO.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,231 次查看
xueweiliu
Contributor I

Thanks!

0 项奖励
回复
3,232 次查看
anthony_huereca
NXP Employee
NXP Employee

Yes, there is no longer a need to drive those pins on 1.1. They can be treated like any other GPIO.

0 项奖励
回复