On Linux (timesys), can you implement pppd?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

On Linux (timesys), can you implement pppd?

跳至解决方案
1,328 次查看
soichiyamamoto
Contributor V

Hi,

On Linux (timesys), can you implement pppd?

Please tell me the method of implementation.

Best  Regards,

soichi

标签 (1)
0 项奖励
回复
1 解答
1,147 次查看
timesyssupport
Senior Contributor II

Hello Yamamoto-san,

Timesys provides the ppp package, which contains the PPP (Point-to-Point Protocol) daemon. If you are using the Web Factory, you can add this package to your web build during the package selection step. If you are using the Desktop Factory, you can run the following command from your top-level Factory directory to include ppp in your build:

make ppp-select && make

Thanks, and let me know if you have any questions.

Timesys Support

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,148 次查看
timesyssupport
Senior Contributor II

Hello Yamamoto-san,

Timesys provides the ppp package, which contains the PPP (Point-to-Point Protocol) daemon. If you are using the Web Factory, you can add this package to your web build during the package selection step. If you are using the Desktop Factory, you can run the following command from your top-level Factory directory to include ppp in your build:

make ppp-select && make

Thanks, and let me know if you have any questions.

Timesys Support

0 项奖励
回复
1,147 次查看
richard_stulens
NXP Employee
NXP Employee

Hi Soichi,

I think that is a 100% Linux question. This community group is dealing more with Vybrid hardware related questions.

You will probably get an answer more quickly on the Timesys forums.

Best regards,

Richard

0 项奖励
回复
1,147 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 项奖励
回复