On Linux (timesys), can you implement pppd?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

On Linux (timesys), can you implement pppd?

Jump to solution
2,294 Views
soichiyamamoto
Contributor V

Hi,

On Linux (timesys), can you implement pppd?

Please tell me the method of implementation.

Best  Regards,

soichi

Labels (1)
0 Kudos
Reply
1 Solution
2,113 Views
timesyssupport
Senior Contributor II

Hello Yamamoto-san,

Timesys provides the ppp package, which contains the PPP (Point-to-Point Protocol) daemon. If you are using the Web Factory, you can add this package to your web build during the package selection step. If you are using the Desktop Factory, you can run the following command from your top-level Factory directory to include ppp in your build:

make ppp-select && make

Thanks, and let me know if you have any questions.

Timesys Support

View solution in original post

0 Kudos
Reply
3 Replies
2,114 Views
timesyssupport
Senior Contributor II

Hello Yamamoto-san,

Timesys provides the ppp package, which contains the PPP (Point-to-Point Protocol) daemon. If you are using the Web Factory, you can add this package to your web build during the package selection step. If you are using the Desktop Factory, you can run the following command from your top-level Factory directory to include ppp in your build:

make ppp-select && make

Thanks, and let me know if you have any questions.

Timesys Support

0 Kudos
Reply
2,113 Views
richard_stulens
NXP Employee
NXP Employee

Hi Soichi,

I think that is a 100% Linux question. This community group is dealing more with Vybrid hardware related questions.

You will probably get an answer more quickly on the Timesys forums.

Best regards,

Richard

0 Kudos
Reply
2,113 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 Kudos
Reply