On Linux (timesys), can you implement pppd?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

On Linux (timesys), can you implement pppd?

ソリューションへジャンプ
1,352件の閲覧回数
soichiyamamoto
Contributor V

Hi,

On Linux (timesys), can you implement pppd?

Please tell me the method of implementation.

Best  Regards,

soichi

ラベル(1)
0 件の賞賛
返信
1 解決策
1,171件の閲覧回数
timesyssupport
Senior Contributor II

Hello Yamamoto-san,

Timesys provides the ppp package, which contains the PPP (Point-to-Point Protocol) daemon. If you are using the Web Factory, you can add this package to your web build during the package selection step. If you are using the Desktop Factory, you can run the following command from your top-level Factory directory to include ppp in your build:

make ppp-select && make

Thanks, and let me know if you have any questions.

Timesys Support

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,172件の閲覧回数
timesyssupport
Senior Contributor II

Hello Yamamoto-san,

Timesys provides the ppp package, which contains the PPP (Point-to-Point Protocol) daemon. If you are using the Web Factory, you can add this package to your web build during the package selection step. If you are using the Desktop Factory, you can run the following command from your top-level Factory directory to include ppp in your build:

make ppp-select && make

Thanks, and let me know if you have any questions.

Timesys Support

0 件の賞賛
返信
1,171件の閲覧回数
richard_stulens
NXP Employee
NXP Employee

Hi Soichi,

I think that is a 100% Linux question. This community group is dealing more with Vybrid hardware related questions.

You will probably get an answer more quickly on the Timesys forums.

Best regards,

Richard

0 件の賞賛
返信
1,171件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 件の賞賛
返信