NOR Boot - Linux + MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NOR Boot - Linux + MQX

ソリューションへジャンプ
3,365件の閲覧回数
bfac
NXP Employee
NXP Employee

Hello!

We are evaluating the possibility of using a Flash SPI memory to boot the whole system on our product, we understand the memory size would be a limitation, but as our product will not have any display and sound we think it should fit a small NOR memory.

We think to boot the whole system from the NOR, so we should have u-boot, kernel, rootfs and mqx images on the memory, at a first analysis it looks feasible, but I wonder if this is already implemented.

The question then is:

Is the boot over SPI NOR already implemented for u-boot?

Our master core is the A5, it should boot the u-boot from NOR, and then u-boot should unpack, store and start M4 core with MQX image on internal RAM. Linux would follow regular u-boot steps to boot from DDR, rootfs should also be on DDR.

Thanks!

Bruno

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 解決策
3,053件の閲覧回数
vladimirkhusain
Contributor III

Yes, this is possible to do. In fact, your configuration appears to be very close to a boot scenario descibed in Chapter 6 of this document:

http://www.emcraft.com/docs/VF6-SOM-skg-1.11.0.pdf

Boot is from a Spansion QSPI Flash device. Target platform is the Emcraft Sstems VF6 System-On-Module Starter Kit:

Vybrid VF6 SOM

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,054件の閲覧回数
vladimirkhusain
Contributor III

Yes, this is possible to do. In fact, your configuration appears to be very close to a boot scenario descibed in Chapter 6 of this document:

http://www.emcraft.com/docs/VF6-SOM-skg-1.11.0.pdf

Boot is from a Spansion QSPI Flash device. Target platform is the Emcraft Sstems VF6 System-On-Module Starter Kit:

Vybrid VF6 SOM

0 件の賞賛
返信
3,053件の閲覧回数
bfac
NXP Employee
NXP Employee

Thanks Vladimir!

What Linux BSP you are using? The timesys one?

0 件の賞賛
返信
3,053件の閲覧回数
vladimirkhusain
Contributor III

Not timesys. We (Emcraft) maintain our own BSP. It is available for free download from our web site so fell free to check the QSPI Flash boot code in U-boot.

0 件の賞賛
返信