NAND flash read performance?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND flash read performance?

ソリューションへジャンプ
2,247件の閲覧回数
zoltanjanosy
Contributor I

Does anyone have any figures for the read performance of the NAND flash controller, when used with 32 bit error correction? I am interested in the added latency of the error correction, including any software overhead (in plain English, how much does it take to do the error correction on a block of memory).

Zoltan

ラベル(5)
タグ(3)
0 件の賞賛
返信
1 解決策
1,804件の閲覧回数
timesyssupport
Senior Contributor II

Hello Zoltan,

On the Vybrid Tower module, we have not yet collected NAND performance statistics, with/without ECC. We only have Rev. E hardware on hand at this moment, our Rev. G is currently unavailable for testing purposes. Once it returns, we can put together some test figures as they apply to the VF6xx Tower module.

Regards,

Timesys Support

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,804件の閲覧回数
billpringlemeir
Contributor V

See: VF6xxx NFC (NAND) module clocking, where I give some numbers and code to improve it.

0 件の賞賛
返信
1,805件の閲覧回数
timesyssupport
Senior Contributor II

Hello Zoltan,

On the Vybrid Tower module, we have not yet collected NAND performance statistics, with/without ECC. We only have Rev. E hardware on hand at this moment, our Rev. G is currently unavailable for testing purposes. Once it returns, we can put together some test figures as they apply to the VF6xx Tower module.

Regards,

Timesys Support

0 件の賞賛
返信
1,804件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport are you available to  help on this case?

0 件の賞賛
返信