NAND Flash selection for Vybrid F series MCU ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND Flash selection for Vybrid F series MCU ?

ソリューションへジャンプ
1,237件の閲覧回数
AhmedShameemM_H
Contributor I

Dear Sir,

We are designing freescale's Vybrid F series MCU based board, from the reference manual we understand that MCU supports for Maximum 3 address cycle NAND Flash for booting.

Can we use the NAND flash which supports 4 address cycle?

Regards,

Shameem

ラベル(1)
0 件の賞賛
返信
1 解決策
1,054件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

My understanding is that only those commands that require up to 3 address cycles will be executed, and the rest of the commands (that require more than 3 address cycles) will be impossible to be executed

I think we should discourage the use of 4 and 5 address cycles NAND flashes for Vybrid

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,055件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

My understanding is that only those commands that require up to 3 address cycles will be executed, and the rest of the commands (that require more than 3 address cycles) will be impossible to be executed

I think we should discourage the use of 4 and 5 address cycles NAND flashes for Vybrid

0 件の賞賛
返信