How to enable i2c1 in device tree for vybrid vf50 (interrupts)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to enable i2c1 in device tree for vybrid vf50 (interrupts)

跳至解决方案
2,724 次查看
sandrostiller
Contributor I

Hello,

I'm trying to enable the 2nd i2c in the device tree for my linux kernel.

I took the entries for the i2c0 and modified them with this result:

i2c1: i2c@40067000 {

  #address-cells = <1>;

  #size-cells = <0>;

  compatible = "fsl,vf610-i2c";

  reg = <0x40067000 0x1000>;

  clocks = <&clks VF610_CLK_I2C1>;

  clock-names = "ipg";

  dmas = <&edma0 0 52>,

  <&edma0 0 53>;

  dma-names = "rx","tx";

  status = "disabled";                                                   

};

...

...

&i2c1 {

  clock-frequency = <400000>;

  pinctrl-names = "default";

  pinctrl-0 = <&pinctrl_i2c1>;

  status = "okay";

};

While starting the kernel prints this message:

[

0.171667] imx-i2c 40067000.i2c: can't get irq number

I think that I must add an "interrupts" entry, but where can I find the correct number?

In my i2c-0 the number 71 was given, in an other device tree i2c-0 got the 103 and the i2c-1 the number 104

Thanks,

Sandro

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
2,131 次查看
timesys_support
Contributor I

Hello Sandro,

You can try using the value "72" for the "interrupts" entry. This can be found in the Vybrid reference manual at table 3-1, Interrupt Assignment, as the NVIC Interrupt ID for i2c1. The other device tree that you link to specifies the GIC interrupt ID values.

Thanks,

Timesys Support

在原帖中查看解决方案

3 回复数
2,132 次查看
timesys_support
Contributor I

Hello Sandro,

You can try using the value "72" for the "interrupts" entry. This can be found in the Vybrid reference manual at table 3-1, Interrupt Assignment, as the NVIC Interrupt ID for i2c1. The other device tree that you link to specifies the GIC interrupt ID values.

Thanks,

Timesys Support

2,131 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Thank timesyssupport

0 项奖励
回复
2,131 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help here?

0 项奖励
回复