Hello,
I'm trying to enable the 2nd i2c in the device tree for my linux kernel.
I took the entries for the i2c0 and modified them with this result:
i2c1: i2c@40067000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,vf610-i2c";
reg = <0x40067000 0x1000>;
clocks = <&clks VF610_CLK_I2C1>;
clock-names = "ipg";
dmas = <&edma0 0 52>,
<&edma0 0 53>;
dma-names = "rx","tx";
status = "disabled";
};
...
...
&i2c1 {
clock-frequency = <400000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c1>;
status = "okay";
};
While starting the kernel prints this message:
| [ | 0.171667] imx-i2c 40067000.i2c: can't get irq number |
I think that I must add an "interrupts" entry, but where can I find the correct number?
In my i2c-0 the number 71 was given, in an other device tree i2c-0 got the 103 and the i2c-1 the number 104
Thanks,
Sandro
已解决! 转到解答。
Hello Sandro,
You can try using the value "72" for the "interrupts" entry. This can be found in the Vybrid reference manual at table 3-1, Interrupt Assignment, as the NVIC Interrupt ID for i2c1. The other device tree that you link to specifies the GIC interrupt ID values.
Thanks,
Timesys Support
Hello Sandro,
You can try using the value "72" for the "interrupts" entry. This can be found in the Vybrid reference manual at table 3-1, Interrupt Assignment, as the NVIC Interrupt ID for i2c1. The other device tree that you link to specifies the GIC interrupt ID values.
Thanks,
Timesys Support