How many simultaneous ADC samples can I take with the Vybrid? Two?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many simultaneous ADC samples can I take with the Vybrid? Two?

Jump to solution
1,291 Views
johnfielden
Contributor IV

Looking at the vybrid data sheet, there are multiple channels for two ADC ports.  But it appears that I can only take 2 measurements at a time.  I would like to use the DMA to store samples in memory.  If I only have one DMA channel available, I'm guessing that I can only take one measurement at a time.  Is there a way to interleave data?

0 Kudos
Reply
1 Solution
784 Views
naoumgitnik
Senior Contributor V

Hello John,

Below is reply from another Community thread:

"Vybrid has 2 ADCs. Each can be synchronized by External hardware trigger support.

If you raise each, for each ADC, with two separate triggers at the same time, 2 ADCs will measure at the same time. For example using Programmable Delay Block (PDB)."

It might be not exactly about what you are asking, but it gave me a hint that you may probably use the Programmable Delay Block (PDB) to interleave data as well, i.e. make the 2 ADCs' data flow through one DMA channel in the synchronized manner.

Sincerely, Naoum Gitnik.

View solution in original post

0 Kudos
Reply
1 Reply
785 Views
naoumgitnik
Senior Contributor V

Hello John,

Below is reply from another Community thread:

"Vybrid has 2 ADCs. Each can be synchronized by External hardware trigger support.

If you raise each, for each ADC, with two separate triggers at the same time, 2 ADCs will measure at the same time. For example using Programmable Delay Block (PDB)."

It might be not exactly about what you are asking, but it gave me a hint that you may probably use the Programmable Delay Block (PDB) to interleave data as well, i.e. make the 2 ADCs' data flow through one DMA channel in the synchronized manner.

Sincerely, Naoum Gitnik.

0 Kudos
Reply