How do I setup a dma channel to output data on SPI?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I setup a dma channel to output data on SPI?

ソリューションへジャンプ
1,954件の閲覧回数
DanKSI
Contributor III

Hi,

I would like to output data on a SPI bus using DMA using the M4 processor of the Vybrid processor.  The data going to the SPI would be from a memory buffer.  The SPI was initiallized using normal MQX functions and verified to function before trying to switch to using the DMA.  When CSR = 1 is run, the DMA appears to go through its process and CSR then is set to 0x80 and no errors are shown in DMA1.ERR or DMA1.ES.  It appears that the FIFO on the SPI are filled with the data, but no data appears to be sent out from the SPI pins.

Sample Source:

#defineSIZE8  0
#defineSIZE16 1

#define SIZE32 2

#define SIZE64 3

//Enable DMA CH Mux1 Clock

CCM_CCGR0 |= CCM_CCGR0_CG5(3);

//DMA1

CCM_CCPGR3 |= CCM_CCPGR3_PPCG8(3) | CCM_CCPGR3_PPCG9(3);

//Enable SPI 2 source for DMA1

DMAMUX2_CHCFG0 = DMAMUX_CHCFG_ENBL_MASK | DMAMUX_CHCFG_SOURCE(11);

SPI2_RSER |= 0x03000000; //Enable DMA request for TFFF (transmit buffer fill flash)

DMA1_TCD0_SADDR = (uint32_t)(writeData.data); //Source Address For Transfer

DMA1_TCD0_ATTR = DMA_ATTR_SMOD(0) | DMA_ATTR_SSIZE(SIZE16) //Modulo and access size for source

| DMA_ATTR_DMOD(0) | DMA_ATTR_DSIZE(SIZE16);//and destination

DMA1_TCD0_SOFF = 2; //source address offset in bytes after each access

DMA1_TCD0_NBYTES_MLNO = DMA_NBYTES_MLNO_NBYTES(writeData.dataSize); //total number of bytes in minor loop (is a multiple of 16 bits)

DMA1_TCD0_SLAST = (writeData.dataSize * -1); //source address adjustment on major loop completion - used to reset TCD

DMA1_TCD0_DADDR = (uint32_t)(&SPI2_PUSHR); //Destination Address For Transfer

DMA1_TCD0_CITER_ELINKNO = 1; //current major count

DMA1_TCD0_DOFF = 0; //destination address offset in bytes after each access

DMA1_TCD0_DLASTSGA = 0; //destination address adjustment on major loop completion - used to reset TCD

DMA1_TCD0_BITER_ELINKNO = 1; //total major iteration count

DMA1_TCD0_CSR = 0; //set all bits to zero

DMA1_SERQ = 0; //set TCD0 enable

DMA1_TCD0_CSR = 1; //start the DMA

Thanks for any help,

Dan K.

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,596件の閲覧回数
DanKSI
Contributor III

I reviewed how the MQX spi functions worked and found that the configuration was only set when doing a RX/TX.  I was no longer using the MQX sending functions, so the configuration was never set.  Either setting the configuration manually or sending some dummy data was enough to make the SPI start sending using DMA.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,597件の閲覧回数
DanKSI
Contributor III

I reviewed how the MQX spi functions worked and found that the configuration was only set when doing a RX/TX.  I was no longer using the MQX sending functions, so the configuration was never set.  Either setting the configuration manually or sending some dummy data was enough to make the SPI start sending using DMA.

0 件の賞賛
返信
1,596件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Dan,

Thank you for sharing your comments!


Regards,
Carlos

0 件の賞賛
返信