High-level input higher than ovdd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

High-level input higher than ovdd

Jump to solution
4,038 Views
shouminliu
Contributor II

Dear Sir or Madam:

we are evaluating multiple options to power the Vybrid using a single 3.3V supply. We are looking into a 1.5V-controlled LDO as the sequencing device shown in the block diagram attached. However, we have some concerns about the Vybrid. Could you please comment on our questions below?

  1. We realize that there will be a little dropout voltage between 3.3V_P and 3.3V_S anyway. In our application, 3.3V_S will power the  Vybrid and 3.3V_P will power some peripheral digital electronics around it. It is possible that a logic-high input (powered by 3.3V_P) is higher than 3.3V_S that powers the Vybrid GPIO. The data sheet says that the high-level input has a max. value of ovdd, which is 3.3V_S in our case. Will a “higher-than-3.3V_S” cause any damage or malfunctions? What do you think?
  2. In the configuration shown in the block diagram, peripheral electronics will be powered on before the Vybrid (3.3V_P turns on before 3.3V_S). In case there are high-level inputs at some GPIO pins before 3.3V_S is on, we guess these inputs will be shunted to the internal 3.3V rail by the internal protection Schottky diodes. If this is true, the Vybrid 3.3V rail is virtually powered by the high-level input minus the voltage drop on the Schottky diodes. Will this phenomenon cause the Vybrid to enter a “partially-powered” state and malfunction?

Please kindly let us know what you think.

Thanks and regards,

Shoumin

Labels (3)
0 Kudos
Reply
1 Solution
3,796 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
3,797 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
3,802 Views
art
NXP Employee
NXP Employee

Q. Will a “higher-than-3.3V_S” cause any damage or malfunctions?

A. Yes, it can cause an excessive input current and even I/O buffer damage.

Q. Will this phenomenon cause the Vybrid to enter a “partially-powered” state and malfunction?

A. Yes, this can cause a malfunction. The general requirement is that no I/O pins must be externally driven until the processor is powered on.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply