Endianess Problem with 64 bit datatype

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Endianess Problem with 64 bit datatype

跳至解决方案
6,094 次查看
karthigeyannata
Contributor III

We are developing software on vybrid processor(A5 core). We are facing issues with the 64 bit data type. When we tried to print the value using printf or sprintf, the values are printed wrongly.

Then we had identified that it is beacause of endian problem. The Lower 32 bit value is placed in upper 32 bit place and so the it is printing big numbers even for small value

for example when we tried to print the value 0x19 of long long int data type, it is printed as 0x1900000000.

Please let us know , how to overcome this issue.

Note : We are using gcc compiler

0 项奖励
回复
1 解答
5,754 次查看
ioseph_martinez
NXP Employee
NXP Employee

Karthi,

I verified this. Is working fine on my side.

I am using: MQX 4.0.2 Beta 1

Compiler: Sourcery CodeBench Lite Edition for ARM EABI from mentor graphics

Example: Hello

So please do the following:

- download Sourcery CodeBench Lite Edition for ARM EABI from mentor graphics GCC compiler

- obtain from your FAE: MQX 4.0.2 Beta 1

- compile hello example using gcc_cs tool chain mentioned above.

- modify and try using long long type.

Let us know your results. Again, the most important step is the toolchain. If the toolchain you are using does not supports the proper printf it will fail.

On my side, IAR, and gcc from CodeSourcery work correctly.

Best Regards,

Ioseph

code:

unsigned long long my64var;

void hello_task

    (

        uint_32 initial_data

    )

{

  my64var = 0x12345UL;

    printf("Hello World\n");

    printf("Hello World\n");

    printf("%llx", my64var);

    _task_block();

}

output:

Hello World

Hello World

12345

在原帖中查看解决方案

0 项奖励
回复
9 回复数
5,754 次查看
ioseph_martinez
NXP Employee
NXP Employee

Hello,

I think the problem is printf and not the compiler. I tried this on IAR compiler and the way words are ordered is the same as in your case.

For example:

tst = 0x10;

tst = tst + 0xffffffff;

tst = 0x000000010000000F

The printf I am using does not supports printing 64 bits. Please check if in your case the printf supports that size.

See the attached picture of my debug session and how the 64bit integer is handled correctly.

5,754 次查看
karthigeyannata
Contributor III

how to fix this issue in sprintf which is library function?...

How to get rid of this issue?

0 项奖励
回复
5,754 次查看
ioseph_martinez
NXP Employee
NXP Employee

Hi,


Can you please give more details on what tool chain you are using?

Are you using Linux Timesys? OS Less or MQX

From which vendor/where you got your gcc-compiler?

Have you check for any compiler options, flags or documentation notes? Your library seems to support at some degree or may be some port from another system.

This sounds similar: Andrés Moré - Re: printf of unsigned long long in ARM processors, please take a look. If the issue comes from gcc codesourcery they will be the best to answer.

0 项奖励
回复
5,754 次查看
karthigeyannata
Contributor III

Hi,


Please find the details.

We are using MQX and using gcc compiler version 4.5.2

Could you please provide your inputs on this ASAP?

Thanks

karthi

0 项奖励
回复
5,755 次查看
ioseph_martinez
NXP Employee
NXP Employee

Karthi,

I verified this. Is working fine on my side.

I am using: MQX 4.0.2 Beta 1

Compiler: Sourcery CodeBench Lite Edition for ARM EABI from mentor graphics

Example: Hello

So please do the following:

- download Sourcery CodeBench Lite Edition for ARM EABI from mentor graphics GCC compiler

- obtain from your FAE: MQX 4.0.2 Beta 1

- compile hello example using gcc_cs tool chain mentioned above.

- modify and try using long long type.

Let us know your results. Again, the most important step is the toolchain. If the toolchain you are using does not supports the proper printf it will fail.

On my side, IAR, and gcc from CodeSourcery work correctly.

Best Regards,

Ioseph

code:

unsigned long long my64var;

void hello_task

    (

        uint_32 initial_data

    )

{

  my64var = 0x12345UL;

    printf("Hello World\n");

    printf("Hello World\n");

    printf("%llx", my64var);

    _task_block();

}

output:

Hello World

Hello World

12345

0 项奖励
回复
5,754 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Hi ioseph_martinez can you  continue with   the follow up of this  case?

This is not solved yet.

0 项奖励
回复
5,754 次查看
jeffreycoffman
Contributor III

You data type wouldn't happen to be IEEE754 double?

0 项奖励
回复
5,754 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

ioseph_martinez  / juangutierrez can you  help on this case?

0 项奖励
回复
5,754 次查看
juangutierrez
NXP Employee
NXP Employee

How are you printng?

Have you tried to use %llu?

    printf("%llu", my64var);

0 项奖励
回复