Endianess Problem with 64 bit datatype

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Endianess Problem with 64 bit datatype

ソリューションへジャンプ
6,104件の閲覧回数
karthigeyannata
Contributor III

We are developing software on vybrid processor(A5 core). We are facing issues with the 64 bit data type. When we tried to print the value using printf or sprintf, the values are printed wrongly.

Then we had identified that it is beacause of endian problem. The Lower 32 bit value is placed in upper 32 bit place and so the it is printing big numbers even for small value

for example when we tried to print the value 0x19 of long long int data type, it is printed as 0x1900000000.

Please let us know , how to overcome this issue.

Note : We are using gcc compiler

0 件の賞賛
返信
1 解決策
5,764件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Karthi,

I verified this. Is working fine on my side.

I am using: MQX 4.0.2 Beta 1

Compiler: Sourcery CodeBench Lite Edition for ARM EABI from mentor graphics

Example: Hello

So please do the following:

- download Sourcery CodeBench Lite Edition for ARM EABI from mentor graphics GCC compiler

- obtain from your FAE: MQX 4.0.2 Beta 1

- compile hello example using gcc_cs tool chain mentioned above.

- modify and try using long long type.

Let us know your results. Again, the most important step is the toolchain. If the toolchain you are using does not supports the proper printf it will fail.

On my side, IAR, and gcc from CodeSourcery work correctly.

Best Regards,

Ioseph

code:

unsigned long long my64var;

void hello_task

    (

        uint_32 initial_data

    )

{

  my64var = 0x12345UL;

    printf("Hello World\n");

    printf("Hello World\n");

    printf("%llx", my64var);

    _task_block();

}

output:

Hello World

Hello World

12345

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
5,764件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Hello,

I think the problem is printf and not the compiler. I tried this on IAR compiler and the way words are ordered is the same as in your case.

For example:

tst = 0x10;

tst = tst + 0xffffffff;

tst = 0x000000010000000F

The printf I am using does not supports printing 64 bits. Please check if in your case the printf supports that size.

See the attached picture of my debug session and how the 64bit integer is handled correctly.

5,764件の閲覧回数
karthigeyannata
Contributor III

how to fix this issue in sprintf which is library function?...

How to get rid of this issue?

0 件の賞賛
返信
5,764件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Hi,


Can you please give more details on what tool chain you are using?

Are you using Linux Timesys? OS Less or MQX

From which vendor/where you got your gcc-compiler?

Have you check for any compiler options, flags or documentation notes? Your library seems to support at some degree or may be some port from another system.

This sounds similar: Andrés Moré - Re: printf of unsigned long long in ARM processors, please take a look. If the issue comes from gcc codesourcery they will be the best to answer.

0 件の賞賛
返信
5,764件の閲覧回数
karthigeyannata
Contributor III

Hi,


Please find the details.

We are using MQX and using gcc compiler version 4.5.2

Could you please provide your inputs on this ASAP?

Thanks

karthi

0 件の賞賛
返信
5,765件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Karthi,

I verified this. Is working fine on my side.

I am using: MQX 4.0.2 Beta 1

Compiler: Sourcery CodeBench Lite Edition for ARM EABI from mentor graphics

Example: Hello

So please do the following:

- download Sourcery CodeBench Lite Edition for ARM EABI from mentor graphics GCC compiler

- obtain from your FAE: MQX 4.0.2 Beta 1

- compile hello example using gcc_cs tool chain mentioned above.

- modify and try using long long type.

Let us know your results. Again, the most important step is the toolchain. If the toolchain you are using does not supports the proper printf it will fail.

On my side, IAR, and gcc from CodeSourcery work correctly.

Best Regards,

Ioseph

code:

unsigned long long my64var;

void hello_task

    (

        uint_32 initial_data

    )

{

  my64var = 0x12345UL;

    printf("Hello World\n");

    printf("Hello World\n");

    printf("%llx", my64var);

    _task_block();

}

output:

Hello World

Hello World

12345

0 件の賞賛
返信
5,764件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Hi ioseph_martinez can you  continue with   the follow up of this  case?

This is not solved yet.

0 件の賞賛
返信
5,764件の閲覧回数
jeffreycoffman
Contributor III

You data type wouldn't happen to be IEEE754 double?

0 件の賞賛
返信
5,764件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

ioseph_martinez  / juangutierrez can you  help on this case?

0 件の賞賛
返信
5,764件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

How are you printng?

Have you tried to use %llu?

    printf("%llu", my64var);

0 件の賞賛
返信