Do I need two USB connection for MFGToolkit?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do I need two USB connection for MFGToolkit?

Jump to solution
2,561 Views
MehmetAliIpin
Contributor V

Dear community,

We have VF3x prototype, which we could program the on board QSPI chips with last MFGtoolkit SW. I noticed that I if I connect only VF3x USB(0), MFGtoolkit gives "no device connected message". If we also connect the openSDA USB, then MFGToolkit can identify the VF3x and can program it. This may be tolerable for prototype;

but for the production, Do I need both USB's?

Best regards.

Labels (5)
0 Kudos
Reply
1 Solution
2,332 Views
kef2
Senior Contributor V

Mehmet,

Is your board powered via OpenSDA USB?

I believe it is not required. I managed to program with MFGtoolkit my own board via USB0. Blank Spansion QSPI memory programs well. There's no OpenSDA on board, USB1 port is not used.

Regards

Edward

View solution in original post

0 Kudos
Reply
3 Replies
2,333 Views
kef2
Senior Contributor V

Mehmet,

Is your board powered via OpenSDA USB?

I believe it is not required. I managed to program with MFGtoolkit my own board via USB0. Blank Spansion QSPI memory programs well. There's no OpenSDA on board, USB1 port is not used.

Regards

Edward

0 Kudos
Reply
2,332 Views
MehmetAliIpin
Contributor V

Dear Edward,

Thank you very much,

Yes I have both USB and a 5 Volt connector; There is only USB power(not openSDA, but USB0 of VF3x) at the moment. Did you use seperate power supply?

Best regards.

0 Kudos
Reply
2,332 Views
kef2
Senior Contributor V

My board is selfpowered, not USB bus powered.

0 Kudos
Reply