Do I need two USB connection for MFGToolkit?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Do I need two USB connection for MFGToolkit?

跳至解决方案
3,831 次查看
MehmetAliIpin
Contributor V

Dear community,

We have VF3x prototype, which we could program the on board QSPI chips with last MFGtoolkit SW. I noticed that I if I connect only VF3x USB(0), MFGtoolkit gives "no device connected message". If we also connect the openSDA USB, then MFGToolkit can identify the VF3x and can program it. This may be tolerable for prototype;

but for the production, Do I need both USB's?

Best regards.

标签 (5)
0 项奖励
回复
1 解答
3,602 次查看
kef2
Senior Contributor V

Mehmet,

Is your board powered via OpenSDA USB?

I believe it is not required. I managed to program with MFGtoolkit my own board via USB0. Blank Spansion QSPI memory programs well. There's no OpenSDA on board, USB1 port is not used.

Regards

Edward

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,603 次查看
kef2
Senior Contributor V

Mehmet,

Is your board powered via OpenSDA USB?

I believe it is not required. I managed to program with MFGtoolkit my own board via USB0. Blank Spansion QSPI memory programs well. There's no OpenSDA on board, USB1 port is not used.

Regards

Edward

0 项奖励
回复
3,602 次查看
MehmetAliIpin
Contributor V

Dear Edward,

Thank you very much,

Yes I have both USB and a 5 Volt connector; There is only USB power(not openSDA, but USB0 of VF3x) at the moment. Did you use seperate power supply?

Best regards.

0 项奖励
回复
3,602 次查看
kef2
Senior Contributor V

My board is selfpowered, not USB bus powered.

0 项奖励
回复