DCU bus priorization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DCU bus priorization

2,591件の閲覧回数
snowholgi
Contributor I

Hello,

Is there a possibility to increase the priority of the DCU on the bus ? Or is there a mechanism like QoS (quality of service) ?

Thank you

Holger

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,440件の閲覧回数
Aubineau_FAE
NXP Employee
NXP Employee

Hi,

DCU has fixed priority level on the bus ("hard-wired" in the manual).

Which part are you using? MPC5606S or MPC5645S?

Vincent

0 件の賞賛
返信

2,440件の閲覧回数
snowholgi
Contributor I

Hello,

I'm using Vybrid PVF65xxx.

After looking at the right place in documentation, I see that QoS is implemented in NIC301 and it has predefined values where DCU has level 14. So it looks like DCU has already highest priority on the bus.

Holger

0 件の賞賛
返信