DCU bus priorization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DCU bus priorization

2,588 Views
snowholgi
Contributor I

Hello,

Is there a possibility to increase the priority of the DCU on the bus ? Or is there a mechanism like QoS (quality of service) ?

Thank you

Holger

Labels (1)
0 Kudos
Reply
2 Replies

2,437 Views
Aubineau_FAE
NXP Employee
NXP Employee

Hi,

DCU has fixed priority level on the bus ("hard-wired" in the manual).

Which part are you using? MPC5606S or MPC5645S?

Vincent

0 Kudos
Reply

2,437 Views
snowholgi
Contributor I

Hello,

I'm using Vybrid PVF65xxx.

After looking at the right place in documentation, I see that QoS is implemented in NIC301 and it has predefined values where DCU has level 14. So it looks like DCU has already highest priority on the bus.

Holger

0 Kudos
Reply