Configuring the DAC: DACREF_1 pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring the DAC: DACREF_1 pin

ソリューションへジャンプ
2,067件の閲覧回数
n00b1024
Contributor III

Hello,

I'm configuring the DAC on the Vybrid, and noticed a reference (Reference Manual, rev4) to DACREF as the voltage input. However, I haven't been able to find this pin on the Vybrid schematic (F-series, RevG), or on Vybrid_Pinout_1.1_-_F_Series.xlsx.

Thanks.

タグ(1)
0 件の賞賛
返信
1 解決策
1,872件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi,

  Those are internal connections to the DAC module.

The following will be in the next revision of the RM:

For this device, external voltage supplied to VREFH_ADC pin is the only reference voltage for DAC reference.

User will need to set up DACx_STATCTRL [DACRFS]=1 to select the valid VREFH_ADC reference.

When DACx_STATCTRL [DACRFS]=0, the DAC reference is connected to an internal ground node and is not a valid voltage reference.

-Anthony

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,873件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi,

  Those are internal connections to the DAC module.

The following will be in the next revision of the RM:

For this device, external voltage supplied to VREFH_ADC pin is the only reference voltage for DAC reference.

User will need to set up DACx_STATCTRL [DACRFS]=1 to select the valid VREFH_ADC reference.

When DACx_STATCTRL [DACRFS]=0, the DAC reference is connected to an internal ground node and is not a valid voltage reference.

-Anthony

0 件の賞賛
返信