Cold temperature boot up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cold temperature boot up

ソリューションへジャンプ
4,314件の閲覧回数
johnfielden
Contributor IV

Hi, on our board, the Tower, and the Phytec boards that we have in our possession, the Vybrid's part number start with a P.  We understand that this means the parts are pre-qualified parts, or pre-production parts.  Are the "P" parts temperature tested or binned?  Are they guaranteed to work over the Vybrid temp range of -40 to +85C?

I ask because we are seeing failures to boot at temperatures between -20C and 0C.  These failures occur on the Tower as well as on our own board design.

John

0 件の賞賛
返信
1 解決策
4,059件の閲覧回数
johnfielden
Contributor IV

Thanks for the response.  We will wait till we get production parts to do further testing at cold temps. 

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
4,059件の閲覧回数
xtrontec
Contributor I

Something else to check when you are testing at -20C to 0C is that the board(s) are in a non-codensing environment - moisture causing shorting problems on your board etc. I am sure that you have this setup for your environmental test chamber and have it all sealed so that no moisture can get in etc. Just my 2 cents.

0 件の賞賛
返信
4,059件の閲覧回数
xtrontec
Contributor I

Maybe check the datasheet (specified operating temperature range) for the main 24MHz crystal used on the Tower System.

0 件の賞賛
返信
4,059件の閲覧回数
johnfielden
Contributor IV

Says -40C.  So is the crystal on our target board.

0 件の賞賛
返信
4,059件の閲覧回数
johnfielden
Contributor IV

Is it possible to get a response on the temperature question?  We're not sure if this is a real problem, or something likely to be seen with the pre-production parts.

Thanks,

John

0 件の賞賛
返信
4,059件の閲覧回数
naoumgitnik
Senior Contributor V

Hello John,

The Prototype parts are not guaranteed, unfortunately. 

Based on our experience, what might help in this case is lowering value of the crystal oscillator loading capacitors to units of pF. Actually, due to the board stray and Vybrid pin parasitic capacitances, you may even try to simply remove them.

In this case, of course, the oscillation frequency will be higher by a few tens of PPM than nominal, but on this stage it might not be critical.

Regards, Naoum Gitnik.

0 件の賞賛
返信
4,060件の閲覧回数
johnfielden
Contributor IV

Thanks for the response.  We will wait till we get production parts to do further testing at cold temps. 

0 件の賞賛
返信
4,059件の閲覧回数
johnfielden
Contributor IV

Production parts fail too.

0 件の賞賛
返信
4,059件の閲覧回数
naoumgitnik
Senior Contributor V

Discussion continued in about Errata 7293 | Freescale Community.

0 件の賞賛
返信